Heavy diesel engines are not only used in power plants. They also lie at the heart of large ships such as container ships or cruise ships (AIDAaura, AIDAvita). Often each cylinder on these engines has its own...Overview
Hydraulic power unit for two-axis tracking of solar collectors. In the solar cells, light energy is converted to electrical energy. With the addition of hydraulic tracking (tilt angle and orientation), the solar radiation...Overview
Screensaver Betamicron®4Overview